Cancel
Showing results for 
Search instead for 
Did you mean: 

CYCLE800 Rotations

Experimenter
Experimenter

How can I force the post to output CYCLE800 when the rotations are at zero degrees?  When the tool axis is equal to the ZM CYCLE800 is not outputted.

 

Thanks,

Jeremy

2 REPLIES 2

Re: CYCLE800 Rotations

Creator
Creator

 Hallo Jeremy,

 

what kind of post do you use?

Any type from OOTB and other examples or self-programmed post?

 

If you have a self-programmed post, you can use a command PB_call_macro any time you need a CYCLE800.

And describing all CYCLE parameters you can apply $mom_out_angle_pos(0) and  $mom_out_angle_pos(1) as follows:

2016-07-15_121944.jpg

 

If you have a post from Siemens examoles, than look at output condition of a block with CYCLE800.

 

I hope, something from written above was useful for you.

 

Best regards

Ashot.

"Imagination is more important than knowledge" - Albert Einstein

Re: CYCLE800 Rotations

Experimenter
Experimenter

Hi Ashot,

 

Thanks for your help.  I was able to figure out the problem.

 

Thanks,

Jeremy

Learn online





Solution Information