Cancel
Showing results for 
Search instead for 
Did you mean: 

Can i use this generated facet body(ipw) as a blank for next operation

Experimenter
Experimenter

I tried it, but it is not selecting this facet body

5 REPLIES 5

Re: Can i use this generated facet body(ipw) as a blank for next operation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Make sure your selection filter is set to facet body (see image), when you try to specify the blank.

 

2015-09-10_12-14-01.jpg

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Can i use this generated facet body(ipw) as a blank for next operation

Experimenter
Experimenter
Thanks

Re: Can i use this generated facet body(ipw) as a blank for next operation

You probably don't need to save it at all.

If the cavity mill operations are in the same workpiece, turn on 3D IPW.

If they are in different workpieces, set the blank geometry type to IPW and select the other workpiece.

Mark Rief
Retired Siemens

Re: Can i use this generated facet body(ipw) as a blank for next operation

Pioneer
Pioneer

What should I do if I want to use IPW create a BLANK GEOMETRY? LOCAL IPW in "The part containing the source for the IPW must reference the same ....: Alerts are called will appear. Local IPW I set up what I want to know.

Re: Can i use this generated facet body(ipw) as a blank for next operation

Can you explain your question some more?

Are you saving an IPW as a facet body? 

 

Or are you using IPW flow with the blank selection on the geometry group?

 

For IPW flow, there are some rules about the components  - search the help for "IPW Source dialog box".

Mark Rief
Retired Siemens

Learn online





Solution Information