Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not start NX12.0.2 post builder.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

When I start NX12.0.2 post builder.

DOS command window shows:

NX/Post Builder Checking License ...

NX/Post Builder Exited Normally.

 

 

14 REPLIES 14

Re: Can not start NX12.0.2 post builder.

Siemens Phenom Siemens Phenom
Siemens Phenom

I would uninstall and reinstall NX...

Re: Can not start NX12.0.2 post builder.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I have reinstalled NX12.0.2, but still the same.

OS is windows7.

Install to directory E:\NX12\

Re: Can not start NX12.0.2 post builder.

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you launching from start menu?

ScreenHunter_01 Oct. 04 07.46.gif

Re: Can not start NX12.0.2 post builder.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Yes.

Re: Can not start NX12.0.2 post builder.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Do you have any MPs installed? (MP0, MP1, or MP2)?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Can not start NX12.0.2 post builder.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I removed my NX12.0.2 then reinstalled nx-12.0.2.mp02.

 

Re: Can not start NX12.0.2 post builder.

Siemens Phenom Siemens Phenom
Siemens Phenom

At this point I would contact GTAC...

 

Re: Can not start NX12.0.2 post builder.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@oitctw11 wrote:

I removed my NX12.0.2 then reinstalled nx-12.0.2.mp02.

 


Did you (proper procedure)

- remove 12.0.2

- reinstall 12.0.2

- then install MP2?

 

Or did you just (not correct)

- remove 12.0.2

- install MP2?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Can not start NX12.0.2 post builder.

Siemens Legend Siemens Legend
Siemens Legend

First thing to do is to look at the syslog (mostly in C:\Temp) to see if NX has experienced any hiccup during license checking.  Yes, there's a syslog created when PB starts.

Secondly, if you have access and write permission to the POSTBUILD\post_builder.bat,

Comment out (rem) the 1st line and add "pause" to the end of the batch script:

 

rem @echo off
@setlocal

...

...

:END
pause

 

Then, run PB from the Start menu again. It would reveal if anything (env variable) is not defined properly which has caused PB to fail.

 

If still no clue, contact GTAC.

Learn online





Solution Information