Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Can on-machine probing check hole and boss location?

Hello,

I have experimented with on-machine probing in the past but I cannot recall if it can check hole and boss locations.  Can anyone verify if it can check locations?

NX 12.0.2
11 REPLIES 11

Re: Can on-machine probing check hole and boss location?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Are you using Renishaws inspection plus sub programs?

If so then yes you can get the location of holes and bosses.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Can on-machine probing check hole and boss location?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Location and deviation from "ideal" location.

Re: Can on-machine probing check hole and boss location?

Yes, the machines I want to probe on have Renishaw programs installed and I successfully tested a simple probing program.

 

I need to make the inspection program in NX and I am not seeing hole and boss location for a sub-type.  There is an operation called probe cylinder but I thought it was just for checking size.

 

Just a reminder, I tested probing a while ago but I currently do not have the license for it so I am unable to check it myself.

NX 12.0.2

Re: Can on-machine probing check hole and boss location?

@joycejo

John-

Are you speaking of the VQC routines by Renishaw?

NX 12.0.2

Re: Can on-machine probing check hole and boss location?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I have heard them caled that.

 

The sub routines are 9814 for boss and bore?

 

Do you have the probing manual from Rennishaw?

 

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Can on-machine probing check hole and boss location?

I see 9814 in the manual and also 9823 but they apear to be used only for size, not location.  Am I missing something?

NX 12.0.2

Re: Can on-machine probing check hole and boss location?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Open Chapter "Output from ..", I dont remember exact name of this Chapter, and you will see all vars, outputted after this sub.
Chapter name is Variable outputs
#185 x location
#186 y loc
#190 x err
#191 y err

Re: Can on-machine probing check hole and boss location?

Phenom
Phenom

All renishaw feature cycles save size, size error, position and position error in variables

 

RenishawVariables.PNG

 

 

 

Re: Can on-machine probing check hole and boss location?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
For different releases output vars may be different. You can start your 9814 on the real cnc and after finished check vars #100...#200. You will understand here location vars or error vars.

Learn online





Solution Information