Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Can't initialize the CAM tutorial

Genius
Genius

Hello

 

I can't open tutorial sample part files, the system just opens a pax file in Notepad every time after I click one of the tutorial icons on the left. It works previously but somehow not working now

Capture.JPG

2 REPLIES 2

Re: Can't initialize the CAM tutorial

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

At some point in time, you've opened a pax file with Notepad and specified Notepad as the default application to open that file type.

Simplest solution is to find a pax file in the NX install and specify the default program as NX to open them.

Anthony Galante
Senior Support Engineer
PhoenxPLM

Re: Can't initialize the CAM tutorial

Genius
Genius

It works, thanks

Learn online





Solution Information