Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't start the license server. I guess it's a license issue

Experimenter
Experimenter

I'm trying to set up a License Server for NX 10 on Windows 7, but I'm running into some problems at this very moment. The License File was generated from the services available at the WebKey Account and it came with the following strings:

SERVER YourHostname COMPOSITE=844544159991 28000

According to the FAQ section in the installation guide, I changed the SERVER line string to my hostname:

SERVER N70428670 COMPOSITE=844544159991 28000

Anyway, when I start the server daemon (lmtools), the debug log file "splm_ugslmd.log" displays the following lines (the irrelevant ones were suppressed):

 

 

16:06:57 (lmgrd) pid 6128

16:06:57 (lmgrd) Done rereading

16:06:57 (lmgrd) FLEXnet Licensing (v11.10.1.0 build 99220 x64_n6) started on N70428670 (IBM PC) (4/9/2015)

16:06:57 (lmgrd) Copyright (c) 1988-2012 Flexera Software LLC. All Rights Reserved.

16:06:57 (lmgrd) US Patents 5,390,297 and 5,671,412.

16:06:57 (lmgrd) World Wide Web: http://www.flexerasoftware.com

16:06:57 (lmgrd) License file(s): C:\Program Files\Siemens\PLMLicenseServer\License.lic

16:06:57 (lmgrd) lmgrd tcp-port 28000

16:06:57 (lmgrd) Starting vendor daemons ...

16:06:57 (lmgrd) Started ugslmd (pid 5360)

16:06:57 (ugslmd) FLEXnet Licensing version v11.10.1.2 build 106212 x64_n6

16:06:57 (ugslmd) Server started on N70428670 for:        

16:06:57 (ugslmd) NX11110 (consisting of:                         NX11110_3d_to_2d_flattener

16:06:57 (ugslmd) NX11110_assemblies NX11110_drafting NX11110_dxf_to_ug

16:06:57 (ugslmd) NX11110_dxfdwg   NX11110_features_modeling NX11110_gateway

16:06:57 (ugslmd) NX11110_grip_execute NX11110_iges NX11110_nx_freeform_1

16:06:57 (ugslmd) NX11110_nx_nastran_export NX11110_nx_sheet_metal NX11110_nx_spsd_stress

16:06:57 (ugslmd) NX11110_nx_spsd_vibration NX11110_pcf_package_file NX11110_pstudio_cons

16:06:57 (ugslmd) NX11110_pv_ugdatagenerator NX11110_sla_3d_systems NX11110_solid_modeling

16:06:57 (ugslmd) NX11110_step_ap203 NX11110_step_ap214 NX11110_ug_kf_checker

16:06:57 (ugslmd) NX11110_ug_kf_execute NX11110_ug_nas_des NX11110_ug_smart_models

16:06:57 (ugslmd) NX11110_ug_to_dxf NX11110_ug_web_express NX11110_ugopen_menuscript)


16:06:57 (ugslmd) Licenses are case sensitive for ugslmd

16:06:57 (ugslmd)

16:06:57 (ugslmd) Wrong hostid on SERVER line for license file:

16:06:57 (ugslmd) C:\Program Files\Siemens\PLMLicenseServer\License.lic

16:06:57 (ugslmd) SERVER line says COMPOSITE=844544159991, hostid is "COMPOSITE=EC5FF79942C6 COMPOSITE=D10CB69775C3"

16:06:57 (ugslmd) Invalid hostid on SERVER line

16:06:57 (ugslmd) Disabling 8 licenses from feature MA_shape_design_bundle(0ACA 2273 A4EC 9C24 )



16:06:59 (ugslmd) EXTERNAL FILTERS are OFF

16:06:59 (lmgrd) ugslmd using TCP-port 54295

16:07:00 (ugslmd) No valid hostids, exiting

16:07:00 (ugslmd) EXITING DUE TO SIGNAL 25 Exit reason 2

16:07:05 (lmgrd) ugslmd exited with status 25 (Invalid host)

16:07:05 (lmgrd) Please correct problem and restart daemons

 

 

 

In order to overcome the hostid situation, I have changed the SERVER line string to:

SERVER N70428670 COMPOSITE=EC5FF79942C6 28000

When I started the server daemon once again, the debug log file “splm_ugslmd.log” reported the following:

 

16:21:05 (lmgrd)

16:21:05 (lmgrd)

16:21:05 (lmgrd) pid 5556

16:21:05 (lmgrd) Done rereading

16:21:05 (lmgrd) FLEXnet Licensing (v11.10.1.0 build 99220 x64_n6) started on N70428670 (IBM PC) (4/9/2015)

16:21:05 (lmgrd) Copyright (c) 1988-2012 Flexera Software LLC. All Rights Reserved.

16:21:05 (lmgrd) US Patents 5,390,297 and 5,671,412.

16:21:05 (lmgrd) World Wide Web: http://www.flexerasoftware.com

16:21:05 (lmgrd) License file(s): C:\Program Files\Siemens\PLMLicenseServer\License.lic

16:21:05 (lmgrd) lmgrd tcp-port 28000

16:21:05 (lmgrd) Starting vendor daemons ...

16:21:05 (lmgrd) Started ugslmd (pid 1620)

16:21:05 (ugslmd) FLEXnet Licensing version v11.10.1.2 build 106212 x64_n6

16:21:05 (ugslmd) Invalid license key (inconsistent authentication code)

16:21:05 (ugslmd) ==>INCREMENT NX1111

16:21:05 (ugslmd) Invalid license key (inconsistent authentication code)

16:21:05 (ugslmd) ==>INCREMENT MA_shape_design_bundle ugslmd 30.0 10-may-2015 8 SUPERSEDE
16:21:07 (ugslmd) License server system started on N70428670

16:21:07 (ugslmd) No features to serve, exiting

16:21:07 (ugslmd) EXITING DUE TO SIGNAL 27 Exit reason 4

16:21:12 (lmgrd) ugslmd exited with status 27 (No features to serve)

16:21:12 (lmgrd) ugslmd daemon found no features. Please correct

16:21:12 (lmgrd) license file and re-start daemons.

16:21:12 (lmgrd)

16:21:12 (lmgrd) This may be due to the fact that you are using

16:21:12 (lmgrd) a different license file from the one you expect.

16:21:12 (lmgrd) Check to make sure that:

16:21:12 (lmgrd) C:\Program Files\Siemens\PLMLicenseServer\License.lic

16:21:12 (lmgrd) is the license file you want to use.

16:21:12 (lmgrd)

 

 

Could someone help me out with this issue?

3 REPLIES

Re: Can't start the license server. I guess it's a license issue

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I see different composite in "header" of topic and in footer... May be problem is here?

Re: Can't start the license server. I guess it's a license issue

Esteemed Contributor
Esteemed Contributor

1) You can't edit the "composite" string in the license file.  You have to run the utility to get your composite ID(s) and get a new license file with the proper one.

 

2) is this a laptop?  Issue could be that on wire you get one ID, on wireless another.  There are articles in uganswer about how to set laptops up so they always use the one ID (typically the wired one, as the wireless ones may not be available it turned off).

 

Hope this helps...Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Can't start the license server. I guess it's a license issue

Experimenter
Experimenter
Thank you Ken. I got a new license file from financial support

Learn online





Solution Information