Cancel
Showing results for 
Search instead for 
Did you mean: 

Can you get rid of a non cutting move in lathe roughing

Valued Contributor
Valued Contributor

I have a part with a groove in it that I have to rough away. I would like to just continue cutting across this area without a retract or rapid move. The groove might be shallower in real life and I would like to avoid removing material rapiding across. I know I can go to the model and use a synchronis modeling tool to remove the groove easily, but would prefer to accomplish this through the tool path or without changing the spun outline geometry.

 

lathe_roughing.jpg

Using NX 8.0.3.4
3 REPLIES

Re: Can you get rid of a non cutting move in lathe roughing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is there an option like "cut across voids" available in the operation you used?

Would be good to know what kind of operation you used to be able to really help you Smiley Wink

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Can you get rid of a non cutting move in lathe roughing

Valued Contributor
Valued Contributor

It is a rough turn OD operation subtype under turning.

 

I would like to know where I can find the "cut across voids"  option. I can't seem to find it.

Using NX 8.0.3.4

Re: Can you get rid of a non cutting move in lathe roughing

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If there is no designed option to do that, here are some more workarounds:

- in your roughing operation, you can add stock value to each single member of a spun outline geometry (not actually editing them)

- you can edit path which is ready and just change "Motion Type" of this fragments to "CUT"

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Learn online





Solution Information