Cancel
Showing results for 
Search instead for 
Did you mean: 

Can you use the diameter of the cutter while choosing points for non cutting moves?

Valued Contributor
Valued Contributor

When you choose points for generic motion or non cutting moves to is it possible to offset the radius of the cutter?  RIght now I have to know the radius or diamter of the cutter and put in an offset based on that value.

Using NX 8.0.3.4
2 REPLIES

Re: Can you use the diameter of the cutter while choosing points for non cutting moves?

When offseting from a point, the problem is what direction to offset? Since there is no "part" there is nothing to go away from. 

 

When you define the points, where are you entering the offset?

 

In Generic Motion, have you looked at the Follow Part Offset subop? This will follow the part solid from a start point to an end point, with a given tool axis.

 

Mark Rief
Retired Siemens

Re: Can you use the diameter of the cutter while choosing points for non cutting moves?

Valued Contributor
Valued Contributor

unfortunately I get a Black X on the motion for follow part offset. Is there something the operation needs to see. I chose the workpiece for the geometry.

Using NX 8.0.3.4

Learn online





Solution Information