Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot Edit the Marker of Canned Cycle in Post Builder

Valued Contributor
Valued Contributor

Hello there,

 

I am trying to edit the Tapping marker of Canned Cycle in Post Builder.

 

Tapping.PNG

 

Normally, I should toggle on the Customize check box in Common Paramter.

 

CommonParameter.PNG

 

But now we have a post purchased from service provider, in which there isn't this option.

 

 

2 REPLIES 2

Re: Cannot Edit the Marker of Canned Cycle in Post Builder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I've seen that using a Siemens 840D controller template.

 

My first tests (if nobody has a better solution)...

1) See if the cycle is defined in a macro call ("macro" tab on the first dialog you show).  See if that can be edited. (if that's what you want to edit)

 

2) Add PB_CMD custom commands to do what you want.  Note you may also have to edit the existing ones.  You may have to MOM_disable_address to "turn off" the output you don't want, then turn it back on later.

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Cannot Edit the Marker of Canned Cycle in Post Builder

Valued Contributor
Valued Contributor

Thanks, Ken.

 

I want to add a condition to the current commands in the Tapping event marker. If the condition is satisfied, run those commands. If not, run a custom command that I will add.

 

Thanks,

Kai

Learn online





Solution Information