Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot build Grid in multi axis VARIABLE_CONTOUR

Pioneer
Pioneer

in multi axis VARIABLE_CONTOUR, when choosen surfaces, it shows can not build grid(drive geometry will be erased). screen shot is attached. tried by reducing the tolerance but no result.  

 

any solution for the attached file?

 

 

 

 

4 REPLIES

Re: Cannot build Grid in multi axis VARIABLE_CONTOUR

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can try to change Chain tolerance, 2mm will be good. But. If first face have a 3corners and second face have a 4corners - it will be impossible. Depends your cut direction you can chose Next Row. If not - extract faces, remove trim. If not - upload your prt. Or send me.

Re: Cannot build Grid in multi axis VARIABLE_CONTOUR

Gears Phenom Gears Phenom
Gears Phenom

Try using Streamline Drive method and select the faces to be machined in the cut area.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Cannot build Grid in multi axis VARIABLE_CONTOUR

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I this is not real part, but sample part for training.

1. With Surface Area strategy will be impossible to mill this part. May be StreamLine will be more better.

2. If you want Surface Area - I try to generate one toolpath for fillet for tool with R1.2 and Tool Axis away from Cylinder Axis.

RUDRA1.pngSurface Area Milling

 

 And second path as Sequential Millind for Ball Mill, normal to part.

RUDRA2.pngSequential Milling

 

 

Re: Cannot build Grid in multi axis VARIABLE_CONTOUR

Pioneer
Pioneer

thanks a lot !

Learn online





Solution Information