Cancel
Showing results for 
Search instead for 
Did you mean: 

Cavity Mill_ Follow Periphery Reliability

Creator
Creator

HI,

Every time i generate a Cavity Mill Program with Follow Periphery, the Tool Path digs into the Part,

Is this a common problem are am I not using the proper settigs.

 

Thanks

 

23 REPLIES

Re: Cavity Mill_ Follow Periphery Reliability

The tool should never dig in to the part. 

If you are seeing excess material removal with the IPW, can you please provide a picture, and indicate the part and blank, and where you think the tool is digging in?

Mark Rief
Retired Siemens

Re: Cavity Mill_ Follow Periphery Reliability

Genius
Genius

Hi,

 

Please check you 'Cutting Parameters' for

1) Island Clean Up

2) Wall Clean Up

 

Sometimes if you don't do this, cutter may dig into uncleaned portion while retract/transfer moves.

BR
Mak
TC10/NX 9

Re: Cavity Mill_ Follow Periphery Reliability

Valued Contributor
Valued Contributor
It is most likely where the tool parameters are set for like a 5/8 diameter with a .125" corner radius and the 2d graphics visual plot is indicating undercutting because the tool path is shifting towards part material boundry based on like a depth .030" of cut and material stock settings stock .03" and the .120" tool radius. strickly visual?
Make shure to use gouge checking when using cavity milling.
EDS UG V3 -UG V15 UNIX; UGS UG V6 -UG V19 - NX-NX5 UNIX/MS; Siemens NX6-NX11 MS

Re: Cavity Mill_ Follow Periphery Reliability

Creator
Creator
The Cutter undercuts the stock.

Re: Cavity Mill_ Follow Periphery Reliability

Creator
Creator

I don't think those options are still available on NX 10.

 

I am migrating to NX 10 from NX 7.5, and i can't find those options anymore

 

Thanks

 

Re: Cavity Mill_ Follow Periphery Reliability

Creator
Creator

I don't think its only Visual, cause i can see the tool path undercutting stock.

 

Re: Cavity Mill_ Follow Periphery Reliability

Siemens Genius Siemens Genius
Siemens Genius

Hi,

 

Which NX version are you useing? Can you upload a simple case showing the issue?

 

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Cavity Mill_ Follow Periphery Reliability

Valued Contributor
Valued Contributor

What is the Visualization Preferences set at in your model?

I set mine to Ultra Fine.

 

Is there a large geometry in/out tolerance?

Is there a large boundry in/out tolerance?

There could be a XYZ discrepency with your tool parameter and tool pattern.

Do you have the Allow under cutting turned on?

Do you have a Milling tool Z Offset in the regestar?

You could have a tool in the operation and a deferent tool selected with the Library reference

EDS UG V3 -UG V15 UNIX; UGS UG V6 -UG V19 - NX-NX5 UNIX/MS; Siemens NX6-NX11 MS

Re: Cavity Mill_ Follow Periphery Reliability

Creator
Creator

Intol outtol: is set to 30 microns.

 

Cut below overhang blank is Off.

 

I have uploaded program info,

 

Thanks

Learn online





Solution Information