Cancel
Showing results for 
Search instead for 
Did you mean: 

Cavity mill Cut levels

Valued Contributor
Valued Contributor

Hello,

 

I would like to teach an operation to my Feature. I want to set in the Cut Levels --> Only at Range Bottom.

 

snip_20170713144805.png

When I teached the operation this setting was not taken in the MKE.  I want that the operation starts at the point of my milling area not at the beginning of the whole feature.

Is there a way to do take this setting into the MKE ?

 

Thank you.

NX 11.0.1.11
3 REPLIES

Re: Cavity mill Cut levels

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For this you need to add one of the two CutLevel add-ons.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Cavity mill Cut levels

Valued Contributor
Valued Contributor

Hello,

 

Thank you. I want to set a Range depth, But the standard measurment is from the Top level.

The Top Level does not measures from my part, it measures from my blank part, which has an offset of 3 mm. Can I change in add-on the measured from into WCS origin ?

 

 

NX 11.0.1.11

Re: Cavity mill Cut levels

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Create a new add-on:

  • Name ... cl
  • Type ... CutLevel
  • Class ... ZLevelBase

Then enter the value:

cl.TopZc = 0.0

This should do it.

See the customization tab for where in the operation dialog you find the values:MKEcustomizationCutLevel.PNGMKE Cut Level Customization

 

 

 

 

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information