Cancel
Showing results for 
Search instead for 
Did you mean: 

Chamfering not possible

Valued Contributor
Valued Contributor

Hi,

 I would like to chamfer this Feature with cavity mill but I get an error.

I dont know how to solve this. I tried with chamfer milling but it does not recognizes the chamfer.

Hope you can help - Thank you

 

snip_20170825111447.png

NX 11.0.1.11
6 REPLIES

Re: Chamfering not possible

Gears Legend Gears Legend
Gears Legend

Don't use Cavity mill for this.

Planar mill is the answer.

-Select boundary > top face > tool outside

-Select floor (same top face)

-Method = Profile

-Cutting > Stock > Final floor stock = -1.5

-Generate

 

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: Chamfering not possible

Valued Contributor
Valued Contributor

Hello,

 

Thank you for your solution.

Actually I forgot to mention, that I want to teach that operation to MKE - so boundaries

are bad because they are not compatible. Is there a way to do that?

 

Thank you Smiley Happy

 

NX 11.0.1.11

Re: Chamfering not possible

Gears Legend Gears Legend
Gears Legend

Another option is to use FloorWall

Now you have to play with floor and wall stock to position the tool correctly

 

 

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: Chamfering not possible

Gears Phenom Gears Phenom
Gears Phenom

planar mill - better is set floor just bellow the chamfer , tool tip will not collide with wall.

 

floor wall - set chamfer as a wall, exact positioning, set z-depth offset to get floor preview jsut bellow the chamfer (again, tool shouldnt collide with the wall)

 

no negative stocks

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Chamfering not possible

Siemens Phenom Siemens Phenom
Siemens Phenom

See attached. Planar Profile is best. You simply pick the curve and set the Drive Point to SYS_OD_CHAMFER. No floor definition necessary.

Re: Chamfering not possible

Valued Contributor
Valued Contributor

Thank you this is very good for me Smiley Happy

NX 11.0.1.11

Learn online





Solution Information