Cancel
Showing results for 
Search instead for 
Did you mean: 

Change C0 B90 to C-180 B-90

Creator
Creator

Dear all

I have problem tool can not cut some area because C Axis collision with part.

When I post NC code output C0. B90. But I need change to C-180. B-90. It's possible to cut.

 

Machine detail.JPG

 

 

Thank you for your reccomend,

Sunny

NX10.0.2

 

2 REPLIES

Re: Change C0 B90 to C-180 B-90

Phenom
Phenom

Try Rotate ude and set C to -180 (or B-90) and check for reference only. If C-180 is in post limits - when NX decides the rotary positions it will be ready to consider C-180 as the closest one.

NX12.02
Windows 10 Pro

Re: Change C0 B90 to C-180 B-90

Creator
Creator

Dear Study

Good idea for edit post.

Thank you so much.

Learn online





Solution Information