Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Change in CSE X-axis to average values in sim13_turn_4ax

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone,
Could anyone advise me how do i change the CSE driver sim13_turn_4ax to simulate the X axis as an average value and no radius?

Thanks to all

2 REPLIES 2

Re: Change in CSE X-axis to average values in sim13_turn_4ax

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

the X Metacode in MCF file calls the method GMe_SetJointValue. Either you overwrite the existing method or the existing X metacode in MCF file by creating your own. 

 

You can move a joint with the CSE kernel command 'SetJointValue'.

 

Thomas

Re: Change in CSE X-axis to average values in sim13_turn_4ax

Siemens Phenom Siemens Phenom
Siemens Phenom

The handling of the X value in CSE for Fanuc interprete as diamter can be set by G10.9 X1 (G10.9 X0 for radius programming which is the default)

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information