Cancel
Showing results for 
Search instead for 
Did you mean: 

Circular interpolation

Creator
Creator

Currently while trying to interpolate circles I am posting in quadrents, is there a setting that allows you to post in full diameter?

5 REPLIES

Re: Circular interpolation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Program & Tool path -> Motion

Click on  the "Circular move" block

In the bottom half of the dialog, set "Circular record" to "Full Circle"

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Circular interpolation

Assuming you have a Post Builder post :*)

Mark Rief
Retired Siemens

Re: Circular interpolation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For Heidenhain controls there is an issue with full circle, if you use arc engage and retract with look ahead enabled (M120 LA).

You will usually end up with only the engage and retract move being performed on the machine.

This only affects contact contour output with cutter compensation enabled, since then it is likely that you need to enable look ahead to stop the machine from barking at the tool path.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Circular interpolation

Genius
Genius
There was issue with output when you change from 'quadrant' to 'full circle' in post builder. Tool used to guage in the part sometimes. I am not sure whether this problem has been resolved or not. See image for clarification.

Re: Circular interpolation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I also have seen issues with arcs when "full circle" is enabled.

ALL my posts output quadrant limited arcs.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information