Cancel
Showing results for 
Search instead for 
Did you mean: 

Configuration of PostProcessor in NX10

Genius
Genius

Hello everybody!

 

Is there a way to get polynomials (e.g. cubic or quintic) as an output of the postprocessor instead of linearly connected points? I am working with NX 10.0.3 and a 5 axis postprocessor for Sinumerik.

 

Thanks in advance!

 

Bye,

 

Flo

3 REPLIES

Re: Configuration of PostProcessor in NX10

Esteemed Contributor
Esteemed Contributor

You need to enable spline output inside of the operation inside of NX under the machine parameters block to get nurbs output.

In addition, you also need the nurbs or Sinumerik spline output license, check your license file for the modules nurb_output_enabler and sinumerik_spline

BTW, when you have the Sinumeric compressor option bought for your Sinumerik controller, you don't need to output splines, since lines and arcs are compressed to splines internally by the controller much better than output by NX.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Configuration of PostProcessor in NX10

Genius
Genius
Thank you very much for your reply!

I found that 'Option' for 3 axis milling but not for 5 axis. Is that working
for 5 axis as well?

I checked the license and found the two modules.

Thank you for your comment on the compressor, I will think about it.

Bye,

Flo

Re: Configuration of PostProcessor in NX10

Esteemed Contributor
Esteemed Contributor

If the option is not available, then the operation doesn't support spline output at all.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Learn online





Solution Information