Cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting NX 7.5 to Teamcenter instance

Experimenter
Experimenter

Hello all,

 

I was wondering if there might be some documentation or if any of you are aware of a way to connect Unigraphics NX to an instance of Teamcenter using the NX command Prompt.

 

Any help would be appreciated

 

Thanks,

 

Koala421

1 REPLY 1

Re: Connecting NX 7.5 to Teamcenter instance

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

NX Help shows this for connecting to a 2-tier environment:

Launching NX in Teamcenter Integration Mode with My Teamcenter

From a command line, type:

$UGII_ROOT_DIR/ugraf —pim=yes —u=<user name> —p=<password>

or

$UGII_BASE_DIR/ugmanager/ugmanager

 

And this for a 4-tier environment.

 

Launching Teamcenter Integration in a four-tier environment

From the command line:

  1. Start the WebLogic software and pool manager application.

  2. Set the environment variable:

    • set UGII_UGMGR_COMMUNICATION=HTTP

  3. Use one of the following three methods to start Teamcenter Integration:

    • set UGII_UGMGR_HTTP_URL=<url>
      ugraf –pim=yes –u=<user> –p=<password>

    • ugraf –pim=yes –http_url=<url> –u=<user> –p=<password>

    • Define the Web Server and Web Server Application Name in the Teamcenter Integration customer defaults (described above).

      • ugraf –pim=yes –u=<user> –p=<password>

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Learn online





Solution Information