Cancel
Showing results for 
Search instead for 
Did you mean: 

Contact Tool Position on Area Milling Boundaries

Experimenter
Experimenter

Hello all,

               I am Arun from india. I have a small query about CONTOUR SURFACE AREA.

I am doing a 3+1 axis machining using contour surface area for a blade profile.

I would like to know in the surface area dialog box, we have an option of TANTO or ON for tool position. I would like to know what are the pluses and minuses of each option. The reason behind is I am getting a smoother toolpath when i use ON function, However I am not sure if this option is going to eat into my profile.

Kindly throw some light on this option.

1 REPLY 1

Re: Contact Tool Position on Area Milling Boundaries

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Tanto means that the drive pathe is calculated with consideration of the tool

On means the drive path is only calculated for the drive surface.

drive_surface1.png

 

If you use part geometry, youre toolpath is likely not to cover the complee cutting area

If you dont use part geometry, youre toolpath will gauge the part.

drive_surface2.png

drive_surface3.png

 

Personally I use tanto for 99%. In some cases -especially when the drive surface is not a part surface it might be better to use on.

 

drive_surface4.png

 

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Learn online





Solution Information