Cancel
Showing results for 
Search instead for 
Did you mean: 

Contour profile - multi depth issue

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello,

 

(nx11.0.2)

 

I want to mill this 360mm tall part in 9 passes.

It generates only 2 or 3 passes.

 Snímka.JPG

What is wrong?

Did I set some parameters wrong?

 

notice: end mill , B angle 30.

When you change the angle to 5 or 10 degrees everything is fine.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
5 REPLIES 5

Re: Contour profile - multi depth issue

Legend
Legend

Maybe at that angle the tool path self intersects,

 

Try turning the collision checking off under non-cutting parameters

 

Paul S.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Contour profile - multi depth issue

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

use the Automatic auxiliary floor. Do not Specify Auxiliary floor.
Then it works

Re: Contour profile - multi depth issue

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

thanks

yes but when tool has smaller B angle it works with specifying auxiliary floor.

I just want to understand why it doesnt work with bigger B tool angle.

 

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Contour profile - multi depth issue

Legend
Legend

Hello

 

When you use contour profile than the tool lenght should be longer than the milled face.

There is an exception. If the angle of the tool is less than as that of the wall.

In this case the tool is internal extended.

So in case of cylindrical tool ther is no problem.

Also in your case when you change the angle to 5 or 10 degrees.

I append your part where the pathes are generated to the top of the part.

I changed only the tool.

 

 

 

Re: Contour profile - multi depth issue

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

thank you for explanation

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information