Cancel
Showing results for 
Search instead for 
Did you mean: 

Coordinate Problem when Import *.stp file.

Pioneer
Pioneer

When I import *.stp file into NX 10.0. The origin XYZ coordinate hasn't been same as Machine Coordinate XmYmZm, and this caused error "the tool not parallel to cutting plane (XmYm) of the part". How can Fix it? Thanks a million!

Untitled
free upload

4 REPLIES

Re: Coordinate Problem when Import *.stp file.

Ken_A 1st Gear
1st Gear

Import it into part "C"

Then add part "C" to your CAM part as a component - you can position it however you want using assembly constraints.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
Apparently I've turned into a gearhead


Re: Coordinate Problem when Import *.stp file.

Pioneer
Pioneer

Ken,

 

Thanks for your reply.

 

I've done that, but there was another problem when I "Add Component". When I create a sketch or do whatever with that imported one. It was unable to snap/ recognize the feature of that part when I created the curve/edges that need to be traced on orginal ones..

Re: Coordinate Problem when Import *.stp file.

Pioneer
Pioneer

Thank you Ken!

 

It has been solved!

Re: Coordinate Problem when Import *.stp file.

Stefan_Pendl 3rd Gear
3rd Gear

When you import any foreign part through a neutral format, you have always to move the imported solid to position it as you like.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Learn online





Solution Information