Cancel
Showing results for 
Search instead for 
Did you mean: 

Coordinates for Mazak

Gears Phenom Gears Phenom
Gears Phenom

hello,

 

Ive never met with this type coordinates.

So how to get these:

-stationary X Y Z.

(X20 Y20 Z0 C... in every move)

...coordinates into XYZ while C is rotating?

mode G43.4.

Snímka.JPG

 

 

I dont know how to get there some transformation (of mcs_gotos or mom_poss) there.

Now I only know how to output tcpm / mcs gotos or mom_poss.

 

Some template for fanuc give such coordinates but there was some problem with accuracy. (-0.2?)

 

We have tried to switch F85 par  0/1 but there was no effect.

 

any Idea?

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
17 REPLIES 17

Re: Coordinates for Mazak

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Juraj,

 

I am guessing you could achieve the same with Lock Axis UDE

Please find attachment and check if it is what you wanted.

I used sim07 post

 

 

Avalon

Re: Coordinates for Mazak

Phenom
Phenom
F85.2 being changed to zero made mine act the way I want (just did it - set to 1 from Mazak.) Type of coordinate system for controlling the tool tip point 0: The table coordinate system that rotates according to the particular rotation of the C-axis is defined as the programming coordinate system. 1: The work coordinate system is defined as the programming coordinate system
NX12.02
Windows 10 Pro

Re: Coordinates for Mazak

Gears Phenom Gears Phenom
Gears Phenom

aaa.jpg

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Coordinates for Mazak

Gears Phenom Gears Phenom
Gears Phenom

Hi  @Avalon,

 

your attachment - when you delete the ude lock, output is the same.

 

But dont know why machined results has somewhere deviation 0,2 and somewhere is OK.

Vericut shows the same deviation.....

So thats why I want coordinates like classic tcpm (m128,traori) to eliminate problem because tcpm wants mcs goto without any transformation etc.

 

Maybe it is caused by some function?

Maybe operators demand on some strange functions.

here is the pre functions which is in program:

G40 G90 G80

M660
G111
G69.5
G0 G28 U0
G0 G28 V0
G0 G28 W0
G30 P2 W0
G53.5
G109 L1

M901
M200
G0 G28 U0
G0 G28 V0
G0 G28 W0
T035.03 T039 M6
M250
G0 B60
M251
G53.5
G17
G98
G97 S0 M203

M902
M300
G110 C2
G28 C0
G0 C0
G111
M901
M200
G0 G28 C0
G0 C0
G97 S0 M203

G110 Z[B]2
Z-500.
G111

M511
G61.1

G98

G122.1
G17
G43.4 H035

(--------------------------------------------)

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Coordinates for Mazak

Phenom
Phenom
Sounds like F85.2 is set to 1. This means that you are programming as if in machine coordinates. So - in a TCP'less way - meaning when you turn the rotary (only) the tool will not try to track a point (move XYZ.) https://www.youtube.com/watch?v=Gs5EKfL95WU
NX12.02
Windows 10 Pro
Highlighted

Re: Coordinates for Mazak

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Juraj,

 

I'm not sure what is the cause but try this header

This has G54 Work offset, so you may want to set it

 

O0001

 

G109 L1

 

 

N10

 

M901

M200

G98 G21 G40 G17 G80

G123.1

G28 U0 V0

G28 W0

G53.5

T001.01 T001 M6

G28 U0 V0 W0

G122.1

M212

M250

G0 B90.

M251

G53.5

G52.5

G54

G122.1

G97 M203 S2000

M250

M212

C0.

G0 G43.4 H1 X98.958 Y-14.4 Z0. B90. C0.

X40.577

G98 G1 X38.895 Y-14.371 F1000.

 

 

Avalon

 

Re: Coordinates for Mazak

Gears Phenom Gears Phenom
Gears Phenom

@Studyhi,

can you show how set F85 properly? maybe operator set it wrong, wrong bit place. some closer explanation of bits.

thanks

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Coordinates for Mazak

Legend
Legend

Hi,
Set F85: 0000 1000

Re: Coordinates for Mazak

Phenom
Phenom
The bit that Frobi shows made it work the way I want (as zero.) There are some that prefer the behavior as set as 1. On round parts it makes it easier to move around the part when set to 1. Frobi, I tried the bit that should switch the Mazatrol to G43.4 P1 (fanuc) or Orivect (Siemens) type of action. In my test it didn't seem to work - even did each rotary move individually. Do you have experience with this?
NX12.02
Windows 10 Pro

Learn online





Solution Information