Cancel
Showing results for 
Search instead for 
Did you mean: 

Copy feeds and speeds from another operation in turning

Master
Master

Just wondering if there was a way to copy the feeds and speeds from one operation to another in turnning operations. I am using NX 8.5. Thanks

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
4 REPLIES

Re: Copy feeds and speeds from another operation in turning

You can inherit feeds from a common method, if that helps.

Mark Rief
Retired Siemens

Re: Copy feeds and speeds from another operation in turning

Master
Master

I thought of that but just wondered if there was a way to do this another way. Kinda like inheret ude's in the operation dialogue. Would be nice

 

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Copy feeds and speeds from another operation in turning

Gears Legend Gears Legend
Gears Legend
Select soms operations and use rightmouse > feeds...
Change the parameters and press ok. Now all operations have the same feeds and speeds😊
Patrick Delisse
KMWE - DutchAero
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.1, TDM 4.8
C#, VB, .NET

Re: Copy feeds and speeds from another operation in turning

Master
Master
That works well in mill but in lathe it changes quite a few feeds get messed up and I am not sure why. Lathe has so many feeds it is crazy to work with.
Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Learn online





Solution Information