Cancel
Showing results for 
Search instead for 
Did you mean: 

Correction G41 in postconfigurator

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

would anyone not know how to set the G41 correction output in the postconfigurator when moving the Z-axis rapid traverse before the ramp? I need this for a machine that loads G41 radius correction at G0 in the z axis.

Thank you

4 REPLIES

Re: Correction G41 in postconfigurator

Legend
Legend

Hello

If it is an Fanuc-Controller there is an setting for this.

pic.png

Re: Correction G41 in postconfigurator

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I've already done it, but it will not do anything. It has no effect on the output.

Re: Correction G41 in postconfigurator

Gears Phenom Gears Phenom
Gears Phenom

Problem is not with the setting of postprocessor.

When you look at cl data/path cutcom is turned on in some moment.

So pp is able to output it then.

Not sooner logically.

 

If cutcom will be in the path before Z rapid move, pp could output it.

So I would ensure that cutcom is generated on NX side.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Correction G41 in postconfigurator

Legend
Legend

Cutcom is generated in NX automatically. Also it is output mostly in an move that is normal to the tool-axis.

If you need another behavior than you must use the UDE Cutcom.

 

Learn online





Solution Information