Cancel
Showing results for 
Search instead for 
Did you mean: 

Could not open part file in NX 7.5 and NX9.

Experimenter
Experimenter

NX 7.5 - NX9.jpgNot able to open part file in NX 7.5 & NX9, getting above error message.

TC10 NX9 + BCT16 Platform
3 REPLIES 3

Re: Could not open part file in NX 7.5 and NX9.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is there a version you CAN open the file in?

If so, I'd try open in that version then "save as" to a different name.

Then do a "file cleanup" and save again to yet another name.

See if either of those 2 files are OK

 

If not, it looks like your file is corrupt.  GTAC *may* be able to help you, but probably not.

 

Is there a backup copy somewhere you can test?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: Could not open part file in NX 7.5 and NX9.

First, you need to confirm in what version the part file is saved.

Start > Siemens n.n > NX Tools > Command Prompt, and enter ug_inspect followed by the path to your part file. 

If the part is saved in the current or older version, it should open. If it does not, contact GTAC to diagnose the problem.

 

Mark Rief
Retired Siemens

Re: Could not open part file in NX 7.5 and NX9.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You could also use the refile_part and ug_inspect utilities to correct some problems with corrupted part files.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information