Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Tool Information

Experimenter
Experimenter

 

1PNG.PNG

How can I creat the tool brand into the following picture

2.PNG 

2 REPLIES

Re: Create Tool Information

Not all of the library parameters are retrieved and stored with the NX tool object, because they are not needed to generate a tool path. This includes parameters like you show here - an additional parameter that has been added to your system by customizing the tool library interface.

Even though they are not saved with the NX tool, these extra parameters can be read directly from the library by postprocessors and shop docs. This may be enough for your requirements. What do you want to use the parameter for?

If you really need the parameter saved with the tool, and in the tool dialog, then you can add it as a User Tool Parameter. Take a look at the file mach\resource\library\tool\ascii\dbc_tool_ud_data_sample.tcl. It has samples of hard coded parameters, and parameters read from the tool database. There is documentation here.

Mark Rief
Retired Siemens

Re: Create Tool Information

Experimenter
Experimenter

Hi Mark

 

Do you have some more information about this topic?

I want include the tool supplier info to my database too but I don't really understand how to do.

 

I hope you can help me.

 

Thank you in advance.

NX 11.0.1 MP2

Learn online





Solution Information