Cancel
Showing results for 
Search instead for 
Did you mean: 

Create and integrate tool for robot ABB

Creator
Creator

Hi! 

 

I made an iron (3D, format igs). I want use it like tool for my robot ABB (model parasolid downloaded from the ABB's website). I have two questions.

 

 What's the steps for add the iron like tool to my robot?

 

Then I want add a third element, maybe a furniture, so, how can I integrate that's three elements (Iron, robot and furniture)?

 

I hope was clear.

5 REPLIES 5

Re: Create and integrate tool for robot ABB

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

In general the process is very much similar to the way you add fixtures and assembly tools to NX CAM.

There are training materials about building robots and using the system that you can access here. I'd recommend to start with those.

 

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Create and integrate tool for robot ABB

Creator
Creator

I can't access to the content... have any cost?

Re: Create and integrate tool for robot ABB

Creator
Creator

I think that following the steps of the video (https://www.youtube.com/watch?v=LHd8pMOaPlU) I can convert my 3D iron as a tool.

Re: Create and integrate tool for robot ABB

Creator
Creator

Hi. Trying to convert my Iron as a tool, I have a doubt. I don't know how to assign the trackpoint geometry for the solid tool. 

 

About the Junctions I need help too. For specify mounting, I selected a point where is the red circle and for the specify tool tip, I selected a point where is the green circle. That's right? 

Re: Create and integrate tool for robot ABB

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

It is hard to understand from the picture if it is right or wrong. basically the mounting junction is the point where the "Tool" is mounted to the robot flange. here you have to make sure that the frame alignment (X, Y and Z directions) fit the pocket at the end of J6. otherwise the tool will be mounted with angle to reality.

The Tool tip junction is the point tracking the tool path. it must be aligned with +X upwards (relative to the toolpath) and Y axis should fit the orientation in reality. this is esential to allow appropriate Tool Path base simulation. in the post configurator interaction you can replace the +X direction with +/- X/Z to fit the expected output.

Apart from the definition of assembly tool you also need the parametric tool definition. when you generate the base toolpath in NX CAM the parametric tool is considered.

All of these are described and escorted with step by step exercise in the training materials I recommended above, but those probably require registration.

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Learn online





Solution Information