Cancel
Showing results for 
Search instead for 
Did you mean: 

Create sync tags in the synchronization manager

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello everyone,

When I create sync tags in the synchronization manager, I create the M100 on the first channel, but M101 is created on the second channel, and when I add the second mark, the M101 is created in the first channel and the M103 in the second channel, and so goes on. Does something have to be added to the post?

Thanks

2 REPLIES

Re: Create sync tags in the synchronization manager

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello pajalin,
thank you for your question.
I forwarded the question internally.
We will follow up as soon as we can.

Cheers,
Alexander

Re: Create sync tags in the synchronization manager

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello pajalin,

 

Please check your code of MOM_sync hnadler in postprocessor.

You can reference PB_CMD_handle_sync_event code in sim15_millturn_9ax_fanuc_mm pp.

 

My assumption is the mom_sync_start is not intialized for 2nd channel.

 

Li Li

Li Li

Learn online





Solution Information