Cancel
Showing results for 
Search instead for 
Did you mean: 

Create tool solid

Experimenter
Experimenter

Hi friends

 

I´m trying to convert to a solid, a tool that I visualize in a toolpath.

Is that posible?

 

Thanks in advance

 

euao

9 REPLIES

Re: Create tool solid

Gears Legend Gears Legend
Gears Legend
This is possible. You have to look in the documentation. It's well documented.
Patrick Delisse
KMWE - DutchAero
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.1, TDM 4.8
C#, VB, .NET

Re: Create tool solid

Gears Phenom Gears Phenom
Gears Phenom

From the Tool view of the operation navigator select the tool.

On the Assembly Navigator you should see the tool you just selected as a component

Right click and select make displayed part. Save the file.

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace Connecticut
www.senioraeroct.com
Production: NX11.0.2.7, Vericut 8.0.3
Development: Tcl/Tk
Testing NX12.0

Re: Create tool solid

Experimenter
Experimenter

Thanks John but something I´m doing wrong.

 

From the Tool view of the operation navigator select the tool.-->OK

 

 

On the Assembly Navigator you should see the tool you just selected as a component--OK

 

 

 

Right click and select make displayed part. Save the file. -->I can´t

tool solid.jpg

 

 

Re: Create tool solid

Pioneer
Pioneer

hi !

 

see attachment Smiley Very Happy

 

Re: Create tool solid

Experimenter
Experimenter

Thanks a lot Pionner

 

But I'm afraid I have bad explained.

 

During the simulation of a toolpath I would like to convert to solid a tool in a position determinated

 

 

 

Thanks agian

Re: Create tool solid

Gears Phenom Gears Phenom
Gears Phenom

May I ask why?  the tool path visualization will display the tool along the path.  What is the end objective?

 

John Joyce, Manufacturing Engineer,
Senior Aerospace Connecticut
www.senioraeroct.com
Production: NX11.0.2.7, Vericut 8.0.3
Development: Tcl/Tk
Testing NX12.0

Re: Create tool solid

Experimenter
Experimenter

 

To use the tool surface in order to make a surface.

 

Thanks

Re: Create tool solid

Gears Phenom Gears Phenom
Gears Phenom

You can run the tool path verification and when the tool get to the location you want you can select Analysis - Measure distance  Set the anotation to Create Line.  Pick two points one at tip of the tool and one the top of the tool.

 

Now you have a line you can use to locate the tool you had saved as previously described.  You can link the body of the tool and use the to model whatever you need.

John Joyce, Manufacturing Engineer,
Senior Aerospace Connecticut
www.senioraeroct.com
Production: NX11.0.2.7, Vericut 8.0.3
Development: Tcl/Tk
Testing NX12.0

Re: Create tool solid

Experimenter
Experimenter
Good Idea

Learn online





Solution Information