Cancel
Showing results for 
Search instead for 
Did you mean: 

Customization shop doc toolist

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I want to customize toolist like this,,,how can i do it...thanks.

 

toolist.png

 

7 REPLIES 7

Re: Customization shop doc toolist

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't think you'll be able to get max/min Z (and possibly other things) using the actual NX "Shop docs" module.

 

I create my "shop docs" like files by saving data while posting and then using regular tcl code to create an HTML file at the end.

 

if you "source" in tcl files to your post, you can use the same code for all posts.  Custom commands ("PB_CMD_*") can be created in the first post you work on, then exported to a tcl file that can then be imported into other posts, so all you have to do is "drag-n-drop" them to the right events/locations.

 

I'm not sure what the new "work instructions" can do.

 

You might want to check & report when different operations (that use the same tool) use different feeds & speeds

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Customization shop doc toolist

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thanks Ken_A,

I add the spindle_speed and feedrate variable to the table, but output not present,,,,

Please see shop docs in attched file.

2016-11-19_083614.png

Highlighted

Re: Customization shop doc toolist

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Anyone help pls!!!!

Re: Customization shop doc toolist

If you turn on the review tool, I suspect you will find that those mom variables are not defined. 

If you are cycling tools in the tool view, there is no speed or feed, because those are stored in the operations. 

Mark Rief
Retired Siemens

Re: Customization shop doc toolist

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Like I (tried to) say - you may have to do this in the POST.

 

I would just create as an HTML document, and ignore Excel.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Customization shop doc toolist

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thanks all,,,I will research.

Re: Customization shop doc toolist

Experimenter
Experimenter

Hello Mark,

I am having problems capturing the feeds & speeds of the first tool, after that no problem using mom_feed_rate, mom_feed_rate_mode, mom_spindle_speed etc.

Any ideas?

 

Thank you,

 

Paul

Learn online





Solution Information