Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Customize the Postprocess Dialog

Creator
Creator

Hi,
I have just started to learn how to customize my own post, one thing I have successfully has done is to automatically open the output NC-file with a external editor (In this case Cimco).

 

But I would like to be able to control if the file should be opened or not with a checkbox inside the postprocess dialog. Just the same way that "List output" works.
Is there a way to and a checkbox to the postprocess dialog?

 

Thanks! Smiley Happy

 

Postprocess.png

3 REPLIES

Re: Customize the Postprocess Dialog

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't think so.

But you could do a couple things (not quite as good, but I know they can be done):

1) Use a TK dialog after posting to ask the user if they want it opened

2) [I think] Use Menuscript and a "ACTIONS/POST" to pop up a dialog with the same question.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Customize the Postprocess Dialog

The dialog cannot be customized.

 

I would put a UDE on the PROGRAM group, like we do with the operatior message.

Then the post can check that.

Mark Rief
Retired Siemens

Re: Customize the Postprocess Dialog

Creator
Creator

Thanks for your help!
I was afraid that it wasn't possible. I think that have a dialog box to come up every time you postprocess can be annoying.

I ended up to control it with a custom UDE Smiley Happy

Learn online





Solution Information