Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Cut region issues in lathe job.


@shags72 wrote:

This all goes away though , no trim point or any containment at all necessary, if I use the plane at angles on the turning workpiece dialogue.

 

Thanks for the help I do appreciate your time. Has anyone else had an issue with auto on a simple part like this not being correct?

 


The automatic spun outline is a great idea, but as you have seen, it can struggle at times. With recent Parasolid updates, you'll find it is better in NX9.

 

This is in fact why we added planes an angles and planes through points. Although they may require a little interaction depending on the part shape, the results are usually rock solid. If you are in 8.5, I would just use planes at angles. 

Mark Rief
Retired Siemens

Re: Cut region issues in lathe job.

Master
Master
Kal,

The stock was set to 0 on both. Except of course on the roughing op.
I will be using the plane option from now on. Thanks for everyones replies.
Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Learn online





Solution Information