Cancel
Showing results for 
Search instead for 
Did you mean: 

Cutting Moves

Builder
Builder
Anybody know that how to change the color of cutting, non-cutting moves and its lines thickness???

By low graphics i cant see all moves as visible
Thanx
11 REPLIES 11

Re: Cutting Moves

Builder
Builder
I wanna this type of toolpath thickness and its visible

Re: Cutting Moves

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The color is changed in the operations, machining methods and/or customer defaults, depending on if the CAM objects existed or not.

There is no way to change the thickness, but you can create an enhancement request at GTAC.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Cutting Moves

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Vora and @Stefan_Pendl,

 

you are able to change the thickness of the toolpath through these settings:

Menu --> Preferences --> Visualization --> Line --> Set checkmark at Show widths

Picture1.png

 

Like Stefan said, the colouring of the toolpaths can be done through methods or in the operation itself. The dialogue is called Path Display Colors:

2018-06-11 09_58_41-NX 12 - Manufacturing.png2018-06-11 10_00_04-Path Display Colors.png

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: Cutting Moves

Builder
Builder
Thanx
@AlexanderFreund

As you say i did change the color
But about thickness i don't understand properly

In this dialogue box different types of pixle width which one i should be use

Re: Cutting Moves

Builder
Builder
If i changed the pixle width as a result only change my 3D model edge thickness not a toolpath thickness

Thanx

Re: Cutting Moves

Siemens Phenom Siemens Phenom
Siemens Phenom

You don't have to play around with the settings. Just set the checkmark and you should see an impact. It should change both, the edge thickness as well as the toolpath thickness. You have to indeed reselect your operation.

 

As you can see in my picture, it worked.

Lead Product Manager - Mold & Die

Re: Cutting Moves

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The problem is that there is no setting to control the width used to display the tool path (thin, normal or thick), you can just change the overall behaviour of NX, not just the one for the tool path display.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Cutting Moves

Siemens Legend Siemens Legend
Siemens Legend

Hi Stefan,

 

Is it really a problem? we probably can add more controls, but need a good reason for that. in which case the existing options are not suficient?

 

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Cutting Moves

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Eddy,

if we compare the two images of the OP from his initial two posts, the required difference should be obvious.

The image in the first post would benefit of a thin line thickness, which should be a session setting. This would then result in a better resolution similar to the image in the second post.

If you have a high resolution display, the problem is not seen.

The difference could also be based on the use of software instead of hardware rendering, but we don't know the OPs visualization settings for NX.

May be we can get a better overview if the following information is provided by the OP:

  • graphics adapter used
  • graphics driver release used
  • NX visualization settings
Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information