Cancel
Showing results for 
Search instead for 
Did you mean: 

Cylinder Clearance Plane

Experimenter
Experimenter

I am using a 3 axis mill with a 4th axis as the rotating chuck mounted on the bed the X axis is the axis of the chuck.

When I set a cylinder as a clearance plane and machine 2 areas in the same axis the movement from one area to the next shows a radial move, but when I postprocess the program, the radial move doesn't show as a G02 or G03, it shows as lots of small rapid movements in Yaxis and Z axis. Can anyone tell me how to make the movement show as a simple movemont rather than lots of small ones.

Is iyt in the operation or in the postprocessor?

 

Thanks

 

Steve

2 REPLIES 2

Re: Cylinder Clearance Plane

Genius
Genius

Maybe change your Traversal feed from Rapid to a feedrate. Arc moves (G02 and G03) have to have a feedrate defined they cannot be rapid.

Mike Diamond, CNC Programmer, Orizon Aerostructures Inc.

Production: NX10.0.3.5, Vericut 8.1.4, ICAM V21
Development: VB.NET, Tcl/Tk
Testing: NX12

Re: Cylinder Clearance Plane

Gears Phenom Gears Phenom
Gears Phenom

Can you share a NC file here?

 

(If you are talking about movements along the cylinder clearence plane - they are lines, not the circle.

And PP interpret it right. )

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information