Cancel
Showing results for 
Search instead for 
Did you mean: 

Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Morning!

Just now I finished one interesting project. My potential customer ask me about postprocessor for 4-axis СТС Machine. And - he want to wrap planar milling and fixed contour operations onto cylinder.

For example - this is a planar milling with visualisation in NX 2D Dynamic (this is animated GIF, I dont know - can you see animation? Click on image.)

2D Milling

 

I build very simple CSE-model for test my ideas and - you can see a "wrapped" tool path:

CSE-simulations

 

Then we load STL (two-heads eagle, from Russian gerb) and generate FIXED CONTOUR tool path to engrave this STL and - wrap onto cylinder:

 

And final result :

 

Final result

11 REPLIES 11

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Valued Contributor
Valued Contributor

Incredible! Robot surprised I am not sure if NX was ever meant to be able to do that sort of thing (my knowledge being very shallow) so I applaud your abilities to get every last little bit out of NX!

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thank you!

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Phenom
Phenom

I agree - always impressed/inspired by your posts.

NX12.02
Windows 10 Pro
ITC Inc.

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

So impressed that forgot to push button "KUDO"? Smiley Happy

 

Thanks!!

Highlighted

Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

What is the option to wrap the plannar milling operation over a cylindrical face.

Kindly show the steps.

 

Thanks

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thanks for your question!

I have two possibilities to "wrap" planar milling operation to cylyndrical (conical, spherical) face.

 

1. UDOP, when inside NX I recalc planar toolpath to 4-axis toolpath. I do it with UGOPEN application

 

 

2. Secon way - I recalc planar toolpath with postprocesor, as in start topic.

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Experimenter
Experimenter

Hi Chigishev,

 

I there any resource to learn to create the UDOP.

Thanks.

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

swami and swamidiyan - is it a same?

You can find few examples in UGOPEN forlder NX.

Re: Cylindrical Interpolation, 4-axis STL (facet body) milling etc.

Experimenter
Experimenter

Yes.

 

Thanks for the guidance. I will check it out.

Learn online





Solution Information