Cancel
Showing results for 
Search instead for 
Did you mean: 

D - cutcom register

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I want to ask how should do proper settings to output cutcom register?

 

My settings:

1. I have generated path witch cutter compensation - output contact data, all finish passes

2. In postbuilder I have this:

 

aaaa.JPG

3.tool settings:

Snímka2.JPG

I still have no output of D.

 

The variable doesnt exists or am I doing something wrong??

 

Thank you

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
11 REPLIES

Re: D - cutcom register

Gears Phenom Gears Phenom
Gears Phenom

What I have had to do is Force out the D on the Cutcom ON event

 

In post builder make a custom command that has MOM_force once D

 

Add that custom command to the Machine Control event Cutcom ON

 

You should now get the D output each time the Cutter Comp is output

 

CUTCOM-ON.JPGCutcom ON

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: D - cutcom register

Gears Phenom Gears Phenom
Gears Phenom

HI,

 

Thanks for reply.

I did the same.

Still any D.

 

ver 11.0.2, generic 5ax TT

 

D is optional and variable  doesnt exists = D is not outputed

Ive  tried output mom_cutcom_adjust_register in every move if it exists = never.

 

I have to use mom_tool_cutcom_register which contains the same value.

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: D - cutcom register

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note there are 2 places you can specify the cutter comp register:

1) In the tool (or operation)

2) In the "Cutter compensation" UDE (variable = "mom_cutcom_adjust_register"?)

 

I forget which is which, but there are 2 variables for this.

However the "OOTB" default in PB is mom_cutcom_adjust_register, so that SHOULD work.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: D - cutcom register

Gears Phenom Gears Phenom
Gears Phenom

 

mom_cutcom_adjust_register is what I have in all my posts.  We define the offset on the Pocket or Tool

 

Have you tried listing the tool path to make sure the CUTCOM/LEFT and CUTCOM/OFF are actually being triggered?

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: D - cutcom register

Gears Phenom Gears Phenom
Gears Phenom

yes,

 sometimes it gives good output, for example D05 and sometimes it gives no output as my customer said.

I will do more tests.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: D - cutcom register

Gears Phenom Gears Phenom
Gears Phenom

It looks this setting has effect on this.

because cutcom register was set in the tool but in operation wasnt check box ON

Maybe this is the problem.

 

Snímka.JPG

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: D - cutcom register

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would second John's suggestion to look at the internal toolpath (right click on operation - toolpath - list, or if editing the operation, the furthest right icon in the "Actions" block)

 

No cutcom (or no cutcom register) there, then you won't get the variable correctly defined in the posted output.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: D - cutcom register

Gears Phenom Gears Phenom
Gears Phenom

I get output G41/42 so cutcom was triggered.(also cls)

I think the problem was checkblock I mentioned above.

 

btw adjust register , H is outputed always.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: D - cutcom register

Legend
Legend

Try these (3) places and format. I get my D everytime it is the value in the cutcom register

 

Word Sequence.gifLinear Motion.gifForce D at Cutcom on.gif

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Learn online





Solution Information