10-24-2014 09:45 AM
Hello,
How do I set the dialog window, while creating
User Events in Operation Navigator,
to come back the same size so
I can see all the text in the window. Every time I stretch the window
out it pops back to the same size. Using NX 9.0.0.19.
I can't find the setting and I'm too lazy to continue to look for it!
This may be a 'feature'?
Thanks
cylinder
10-24-2014 01:23 PM
The width if the User Defined Events dialog is remembered within the session.
Once you stretch it wider, it will remember that for any operation or part until you exit NX.
10-24-2014 01:33 PM
Sorry Mark,
But it is NOT doing that. That why I thought it was controlled by a setting.
And that's why I said "may be a feature" Is it working for you in 9.0.0.19?
Should I report to GTAC?
Cyl
10-24-2014 03:49 PM
cyl wrote:
But it is NOT doing that. That why I thought it was controlled by a setting.
And that's why I said "may be a feature" Is it working for you in 9.0.0.19?
Should I report to GTAC?
I would clear the dialog memory, and if the problem is still there, contact GTAC. I tried it in 9.0.3. GTAC can run a release to match yours.
10-24-2014 03:54 PM
Thanks Mark .. I'll try that.