Showing results for 
Search instead for 
Do you mean 
Reply

DRILL RETRACTION

HI ALL,

 

I am trying to use SIMPLE DRILL operation.  Secified the hole i want to drill using "generic point."

I have specified my tool axis using "two points."  for cycle type i am using peck drill, with minimum clearance of 200mm. When I generate the toolpath. it generates fine. WHen I verify the toolpath it does what i want it to do. When I go to simulate the toolpath, drills to the bottom of the hole fine but then it is not retracting on the vector it went it. It retracts Z0 (straight up). Anyone have a clue why it generates fine and verifies fine but does not simulate properly?  Anyhelp would be great!

 

DBFOSTER24

1 REPLY

Re: DRILL RETRACTION

The first thing I would recommend is using the hole_making operations instead of drill, since the old point-to-point operations are being retired.

If you want to stick with this operation, then what is your clearance plane? What machine are you simulating with?

Mark Rief
Retired Siemens

Learn online





Solution Information