Cancel
Showing results for 
Search instead for 
Did you mean: 

Danger in simple drill regarding clearance point and r point

Pioneer
Pioneer

Hello friends

if by mistake i define clearance lower then r point in dril i have crash.

can siemens add to drill operations condition that if clearance lower then r point the system will refuse and alarm will show and ask me to fix clearance height?

thank you

 

ps 

1 photo of toolpath with arrow is the dangerous in action.

 

AmnonScreenshot 2016-02-23 13.22.06.png

3 REPLIES

Re: Danger in simple drill regarding clearance point and r point

Phenom
Phenom

That is an older PTP drilling operation type. 

 

You might want to look at this:

http://solutions.industrysoftware.automation.siemens.com/view.php?si=sfb-nx-5691

 

The chances of any updates to change the PTP code are slim at best.

 

It would be possible to add a check in the post for this condition.

 

Or run the visualization and check for gouges and collisions

 

I would add that in some cases eg Back Boring the retract point can be below the drill point etc

Re: Danger in simple drill regarding clearance point and r point

As said before, point-to-point operations are on critical maintenance.

A new user should start with hole making, and never look at the old drilling. 

 

Out of the box, the clearance should be set in the MCS to a safe distance above the part. This is then used by all the operations under it in the geometry view. 

Mark Rief
Retired Siemens

Re: Danger in simple drill regarding clearance point and r point

Pioneer
Pioneer
Hello
hole making is slow, old drill is very fast to program.
thank you for your reply

Amnon

Learn online





Solution Information