Cancel
Showing results for 
Search instead for 
Did you mean: 

Define approach move after local return

Pioneer
Pioneer

Is there a way to control how the tool returns to the cut when using Local Return in turning? I have my return path on a facing path set to clear axial. I would like it to return to the cut by moving radially first then axial. Right now it is making a direct motion. I am using NX 9

 

Thanks in advance!

 

 

NX 12.0.0 PB 12.0.0
7 REPLIES 7

Re: Define approach move after local return

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

Try to go to the geometry view, then expand all items in it. double click Avoidance, on the avoidance dialog box you can control the engage and return of the tool, see the image.

 

turning.JPG

 

hope this helps.

 

Regards,

Jahnsen

Re: Define approach move after local return

Pioneer
Pioneer

Thanks for the reply,

 

I have been trying different settings both in Avoidance and in Non-cutting moves but nothing seems to change the path that the return move makes. My initial approach move changes but not the one in the local return. I'm hopefully just missing something. This is what my scenario looks like. The red line if what I am hoping to get the motion to look like. My local return is set to Clear Axial.

 

Capture.PNG

 

NX 12.0.0 PB 12.0.0

Re: Define approach move after local return

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Have you tried this?

return point.JPG

Re: Define approach move after local return

Pioneer
Pioneer

That changes the final retract of the toolpath but does not change the local return.

NX 12.0.0 PB 12.0.0

Re: Define approach move after local return

Pioneer
Pioneer

Just thought that I would share my findings....

 

I called GTAC with this issue and currently there is no way to achieve this. I am submitting an Enhancement Request for this feature.

NX 12.0.0 PB 12.0.0

Re: Define approach move after local return

Siemens Creator Siemens Creator
Siemens Creator

I have a similiar issue with Local Return where comments show up in the CL file but not after posting.....

DISPLY/CLEAR CHIPS OUT OF BORE

THxs! Ray

Re: Define approach move after local return

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

RE: DISPLY/

Have you tried turning on the (post) review tool & posting this operation, then seeing what happens with DISPLY/?

 

I'm guessing the post isn't handling it correctly.

 

Does DISPLY/ work correctly if it is added elsewhere (e.g. start or end events)?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information