Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Design features shown while exporting 3D tool assembly to tool library

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Haven't had a need to do this myself, so was more talking about the general issues NX can offer the user.

If you followed the instructions of the NX documentation, it could be a bug and should be reported to GTAC.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Design features shown while exporting 3D tool assembly to tool library

Ok, after these days working with this probe that I made, I finally figured out what the issue is here. Forgive my ignorance if that is too obvious for the experts, but I do want to share the solution here, in case someone else comes across this problem.

 

1) Create a tool and place all the auxillary geometries into one layer other than the work layer. Note that it doesn't matter which layer number that you put the geometries to. You can place the geometries to layer 2 or layer 100, what have you. 

 

1.PNG

 

2) Export the tool to library.

 

3) Retrieve your tool in manufacturing environement. Now you may see your auxillary geometries showing up in tool preview, even though you hide them in modelling.

 

2.PNG

 

4) Resolve the problem by doing the followings

    (a) Highlight the tool 

    (b) Click on layer setting

    (c) Make the layers that contain auxillary geometries invisible.

 

3.png

 

4.png

 

Stephan

Highlighted

Re: Design features shown while exporting 3D tool assembly to tool library

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
It would be nice if only the "model" reference set was used.
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Learn online





Solution Information