Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Difference between License Tools of NX vs. Siemens PLM License Server

Legend
Legend

Hi,

 

I couldn't find a better forum within the community. Nevertheless, with the risk of being in the wrong forum I post my question here.

 

When NX is installed there is a "lmtools" command in the Startcenter.

What is the difference between "lmtoos" of NX and the "lmtools" of the Siemens PLM License Server?

 

Do I need to install the Siemens PLM License Server for a NX CAM EAP test license at all?

 

Best wishes,

Joachim

Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5
2 REPLIES 2

Re: Difference between License Tools of NX vs. Siemens PLM License Server

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

They are (more or less) the same file.  (depends on exactly what version of the SPLM license server you installed, vs. the version installed on the client)

 

As long as they are "reasonably" close (and in your case, as I believe you just installed everything, they should be) you should be able to use the (client) lmtools to view the server (e.g. check license usage or whatever).

 

RE:

Do I need to install the Siemens PLM License Server for a NX CAM EAP test license at all?

 

I don't know (I've not done any EAPs) but this *should* be covered in the EAP instructions.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Difference between License Tools of NX vs. Siemens PLM License Server

Legend
Legend
Thanks a lot, Ken.
Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5

Learn online





Solution Information