Cancel
Showing results for 
Search instead for 
Did you mean: 

Difference feed and speed in same tool name

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi All

I have create tool in library.

Such as 

Tool name STD0.1A in "End Mill (non indexable)" and I create same name in "End Mill (indexable)"

I update each difference parameter tool in "Edit Machining Data Libraries"

7-10-2017 8-33-08 PM.jpg

When I load those tools to use. Parameter will read from first parameter tool only.

for this case i dont use "Machining data" to create parameter becuase I need to fig parameter for each tool. 

Thank you.

NX11.0.2

Windows 10

 

2 REPLIES

Re: Difference feed and speed in same tool name

Stefan_Pendl 3rd Gear
3rd Gear

Since the library reference is not unique this is really a user error.

You cannot specify two separate tools with the same library reference, since it is mandatory to have it unique.

I think that NX will not allow you to export two tools with the same library reference and you should never do such things through a text editor.

If you cheat, then the system will not work as expected.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Difference feed and speed in same tool name

@Stefan_Pendl is correct. The libref must be unique. These are different tools with different materials.

I always recommend NOT to try to use the name or libref to describe tool parameters.

Mark Rief
Retired Siemens

Learn online





Solution Information