Cancel
Showing results for 
Search instead for 
Did you mean: 

Different Template Presets in NX8.5/NX10

Valued Contributor
Valued Contributor

Hello! I've noticed that there are different presets in NX8.5 and NX10 with the same Template. We use a mill_planar-Template from NX8.5 In NX8.5 the preset in PLANAR_MILL / Specify Part Boundary / Mode "Curves / Edges" is

 

2016-03-18 12_56_29-Create Boundary.png

 

The same in NX10 is

 

2016-03-18 13_01_12-Create Boundary.png

 

It's really the same Template.

Why?

 

Thank you for help.

 

Werner

Werner
Production: NX10.0.3, FBM | TcUA 10.1.2.2
Development: VB.NET, Tcl/Tk | Testing: NX12.0
5 REPLIES

Re: Different Template Presets in NX8.5/NX10

Esteemed Contributor
Esteemed Contributor

I've never seen that setting default to "open"

(although I don't have NX8.5 loaded to look at what that setting is "as installed")

 

*as a guess* someone edited your template part in NX8.5

 

(assuming you are metric, substitute "english" for metric if not)

I would open up the NX8.5 %UGII_BASE_DIR%\MACH\resource\template_part\metric\mill_planar.prt

and do a Menu -> Information -> Part -> Part history to see who saved it last.

 

Are you saying you copied the file to the NX10 install tree and it has changed?

Are you running any MR or MP for NX10?

I would check to see if there is a mill_planar.prt in the %UGII_BASE_DIR%\MACH\updates (there is in my install - I have MR3 and MP1 installed) - I'm guessing the "updates" folder one is over-riding your file.

 

You can either disable updates (not sure how, I know I ran across it somewhere, maybe the docs? - probably setting an ENV would do it) or copy the \updates\ folder file and fix it.

 

This illustrates one of the dangers of editing the Siemens supplied files.

If *I* were to have wanted to edit the template prt, I would have copied it to (for example) "jobe_mill_planar.prt" and edited it there.  Then point the .opt file at the new file name.

 

Ken

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Different Template Presets in NX8.5/NX10

Valued Contributor
Valued Contributor

Ken,

 

you can disable the templates in the updates-folder by deactivating the following option in the Customer Defaults

(File->Utilities->Cutomer Defaults->Manufacturing->General->Sofware Updates->Use latest Updated Templates)

 

 

Peter

 

Re: Different Template Presets in NX8.5/NX10

Exactly what steps do you take to get to the boundary dialogs pictured? 

Group or operation type? Boundary type?

Mark Rief
Retired Siemens

Re: Different Template Presets in NX8.5/NX10

Esteemed Contributor
Esteemed Contributor

This dialog is not customized through a template part, it is always customized through the customer defaults for boundaries.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Different Template Presets in NX8.5/NX10

Valued Contributor
Valued Contributor

Hello!

 

Thank you Stefan, this is what I wanted to know. In deed it comes from a Customer Default:

 

2016-03-19 07_23_31-Customer Defaults.png

 

In NX8.5 here we have "Open".

 

Thanks a lot.

 

Werner

Werner
Production: NX10.0.3, FBM | TcUA 10.1.2.2
Development: VB.NET, Tcl/Tk | Testing: NX12.0

Learn online





Solution Information