Cancel
Showing results for 
Search instead for 
Did you mean: 

Disappear Button "Simulate G-code from file"

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

NX 12.0.2.9 - and I cannot find menu item Tools-Simulate G-code from file....

 

Command Finder cannot help me.

5 REPLIES 5
Highlighted

Re: Disappear Button "Simulate G-code from file"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Chigishev ,

 

Are you looking for this: Simulate Machine Code File

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Disappear Button "Simulate G-code from file"

Phenom
Phenom
Now there is just one simulate and then when it opens in the ribbon you can select "Tool Path Based Simulation", "Machine Code Based Simulation" or "External Program Simulation". You can set one as default in customer defaults. For right click simulate (post on the fly) you want "Machine Code Based Simulation".
NX12.02
Windows 10 Pro
ITC Inc.

Re: Disappear Button "Simulate G-code from file"

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Thanks! I found it.

But in past it was more better.. I spend a lot of time to change NC-programm, I must usecProgramm manager, long mouse motions to buttons Play and Stop......

Re: Disappear Button "Simulate G-code from file"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Yuri,

 

there is a TechTip video which explains the changed workflow:

https://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX-Manufacturing/External-P...

 

Hope that clarifies the confusion ;-)

 

Thomas

Re: Disappear Button "Simulate G-code from file"

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thanks, @thomasfeind !

Learn online





Solution Information