Cancel
Showing results for 
Search instead for 
Did you mean: 

Divide Toolpath Based on Depth of Cut

Valued Contributor
Valued Contributor

Hi, as the title suggests, I was wondering if there was a way I could divide tool path based on Depth per Cut?

 

Thanks. 

8 REPLIES 8

Re: Divide Toolpath Based on Depth of Cut

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi,

 

Did not find the direct method ... will wait for experts to answer.

 

What if you have cutting tools of different length and divide the toolpath based on the holder? Just a suggestion.

 

Regards

Amit

Re: Divide Toolpath Based on Depth of Cut

Valued Contributor
Valued Contributor
The idea was to create a cavity mill operation and automatically set the step heights. After I generated the path I'd then divide the path based on the cut levels. I could then rearrange the divided operations into the correct order. With IPW turned on I could make this do bottom up roughing in a few click and drags.

Re: Divide Toolpath Based on Depth of Cut

You are asking to divide a path by cut levels. There is no command for this, but you can probably do it with time or distance, assuming there are non-cutting moves between the levels. 

For a starting point, look at the length of the path in the Operation Navigator column, and the number of levels, and estimate the length of the smallest level. Do Tool Path > Divide, select a length about that of the smallest level, and a very large tolerance. The system tries to divide the path at non-cutting moves if it finds them within the tolerance, so by setting a large tolerance, the system will divide the path between the levels.  

For example, a cavity milling operation is 5000 mm long and has 5 cut levels about the same size. Divide the tool path, set the length to 1000, and the tolerance to 80%. You may have to adjust a little, but I think you can what you want.

If this does not give you what you want, the API has access to the cut level markers, so you could write a program to edit the tool path.

Mark Rief
Retired Siemens

Re: Divide Toolpath Based on Depth of Cut

Valued Contributor
Valued Contributor
I don't know how to write a program but I will definitely give your first suggestion a try. Thanks

Re: Divide Toolpath Based on Depth of Cut

Legend
Legend

Sounds like its time to fork over a node locked volumill license Smiley Happy

 


Dennis Rathi
Creations Unlimited

Re: Divide Toolpath Based on Depth of Cut

Valued Contributor
Valued Contributor

Haha, I've definitely given it a thought. I just know Siemens is working on their own version of adaptive clearing so I'm holding out until then. I've been fortunate to test what they have released so far and I'm impressed with what they have done in a short time. Besides a few hiccups here and there, I like the path they have been able to generate.

Re: Divide Toolpath Based on Depth of Cut

Legend
Legend

Ive been using / testing as well but they already said they arent going to do a bottom up roughing option (atleast not right away)

 


Dennis Rathi
Creations Unlimited

Re: Divide Toolpath Based on Depth of Cut

Siemens Legend Siemens Legend
Siemens Legend

I won't lose hope for buttom-up in adaptive milling..

 

Anyway, back to the question opened the discussion - buttom up is more than rearanging existing cut levels. With top-down you have the same coverage with every level. With bottom up the 1st level (at the bottom) already cuts some / all the material avove. Therefore maintaining the entire upper level(s) would result with a lot of air cutting and significatly reduce the attractiveness of bottom up.

As Mark said - the way to acomplish such would be by NX Open trigerring the level markers, But I wouldn't go there.

 

Yours,  

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Learn online





Solution Information