Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Drill Cycle_Cam option

Pioneer
Pioneer

Hello,

Does someone knows what means "cam" option in drill and tap cycle in NX?Capture232.JPG

 

Thanks!

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
2 REPLIES 2

Re: Drill Cycle_Cam option

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Documentation explain this as you see on picture below.

But I prefer to use it differently - as an addition to an "option". So if machine cycle have some specific parameters, which are not supported by any OOTB options in drilling operation - I can use CAM to set some values.

 

cam.png

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Drill Cycle_Cam option

The original purpose was to indicate the depth stop on a 2.5 axis mill - something from the 1970's.

But as @Marek_Pawlus said, if you have a 3 axis mill, you can use it for whatever you want.

Mark Rief
Retired Siemens

Learn online





Solution Information