Cancel
Showing results for 
Search instead for 
Did you mean: 

Drilling depth

Valued Contributor
Valued Contributor

Hi,

I was wondering if there was a way when setting a manual depth for a drilling operation, if I could set the depth based on the top of the workpiece, not the depth of the hole from the start of the hole. When doing deeper holes and trying to figure out tool clearances, this would be most helpful. 

Thanks. 

5 REPLIES 5

Re: Drilling depth

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you use drill operation you can set any depth manually.

Re: Drilling depth

Legend
Legend

Hi Imperial,

 

I think from NX10.0.3 and NX11.0.0 on in Feature Geometry of your operation you can change the Control Point from In-Process... to Machining Feature. Then you machine the hole from the start of the feature independent of IPW.

 

I have no NX at hand, but am quite sure this should be it. (If I understood you correctly)

Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5

Re: Drilling depth

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can use the 3D IPW in the feature geometry dialog of the drilling operations to drill from the blank body.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Drilling depth

Legend
Legend

Hi imperial,

 

Stefan is right. I just overread something in your post.

Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5

Re: Drilling depth

Valued Contributor
Valued Contributor
The blank at the point is the same as the part. I'll have to make a demo of what I'm talking about.

Learn online





Solution Information