Cancel
Showing results for 
Search instead for 
Did you mean: 

Drive Geometry Missing, But tool path can be displayed

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

 I have one PRT file with tool path. When I use higher NX version to open this PRT file, Drive Geometry Missing, But tool path can be displayed. I do not know why?

 

 

Dalishen.pngdalishen2.png

2 REPLIES 2

Re: Drive Geometry Missing, But tool path can be displayed

Legend
Legend
What is the last Version of NX which is working?

Before you go into NX CAM you can set the Chaining Toleranz to an higher value


Re: Drive Geometry Missing, But tool path can be displayed

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The tool path is stored inside the operation.  Note you can "right-click on the operation" -> Toolpath -> Delete

So while you may not be able to generate the operation, you can replay/post process it.

 

The real issue is why the drive geometry goes missing.

I would suggest reporting this issue to GTAC or your VAR, to figure out why.

 

NOTE: Assuming the part (model) geometry is in a separate part file (a component of the NC program part), please verify you are opening the same model component in both versions of NX. (i.e. check your load options, or open the modle geometry component FIRST, then the NC program...)

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information