Cancel
Showing results for 
Search instead for 
Did you mean: 

EDIT TEXT

Pioneer
Pioneer

Hi,

 

Please forgive my frustrated sounding post. I have only been using NX10 for a year. Upgraded to NX11 upon release. So i am still faily new to the NX game and there is still alot of things I don't know and need help with. So I am here! One thing on my list is Bulk editing text in manufacturing. A simple tool/ button called "TEXT EDIT/FIND REPLACE" needs to be added if not already. Notepad has it, Excel has it, and I'm sure a bunch of other CAD/CAM and less expensive softwares have it.  Is there a text edit tool somewhere that I dont know about?  I have alot of toolpaths to rename and its not just a matter of naming them 1,2,3,4,5,ect,.  Also, I am not a VB programer, so if doing coding is a solution,  you will have to be very thorough in your response.

Any help would be great!

 

Best,

 

DBFOSTER24

4 REPLIES 4

Re: EDIT TEXT

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Lets make sure we are talking about the same thing. 

Do you want to rename a bunch of operations on the operation navigator or exit posted output?

 

If you want to rename operations there is a sample journal for that - look in

C:\Program Files\Siemens\NX 10.0\UGOPEN\SampleNXOpenApplications\.NET\CAM\RenameOperationsOntSelection.vb

 

to use this

1. select the operations you want to rename

2. enter the text you want to replace

3 enter the new text

4 click OK

 

 

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: EDIT TEXT

Pioneer
Pioneer
camster,

Thank you! I have never used journals before. This just blew my mind. I had to change the amount of characters used in RenameOperationsOntSelection.vb file. Then it worked perfectly. I definitely don't know a lot about editing VB code so this will take some practice.

Thanks again for the help!

DBFOSTER24

Re: EDIT TEXT

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

You can take this to the next step and create a button to do this.  Look in the help under

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: EDIT TEXT


@dbfoster24 wrote:
camster,

Thank you! I have never used journals before. This just blew my mind. I had to change the amount of characters used in RenameOperationsOntSelection.vb file. Then it worked perfectly. I definitely don't know a lot about editing VB code so this will take some practice.

Thanks again for the help!

DBFOSTER24

I knew @joycejo pointed you in the right direction. Good catch on the characters - this journal was written before the name length was expanded. As you see, if you have a good starting point, even a non-programmer can usually edit a journal to suit. 

This is one of my favorite journals, always on my ribbon. If you add it to your ribbon, try the icon ont_o_rename.

my_journals_on_ribbon.jpg

Mark Rief
Retired Siemens

Learn online





Solution Information